Hi,
Can we use a DDR3L from Winbond with part number W634GU6NB-11 (Speed bin 1866) with STMPU STM32MP1ADD3.
As STM32MP1 datasheet suggest that it can support up-to 1066. So using above part from Winbond will have any interface issue ?
Thanks.
H...
Hi @Community member , Is there any common Linux image available for accelerating STM32MP1 based SoM, irrespective of eMMC (JEDEC Version 5.0/5.1 Complying) & DDR3 manufacturer.
Hi, I tried burning my STM32MP1 board with existing "FlashLayout_emmc_stm32mp157a-ev1-trusted.tsv" file but it throws following error - Error: TSV files are only supported for STM32MPI'm using onboard eMMC (From Kioxia) and STM32MP157AAD3 chip from S...
@hello,
I was using STM32Cubeprogrammer for long time but suddenly Its main function of browsing and selection file option (OpenFile) stopped working. After multiple time install and uninstall it has the same behavior in a particular PC. I tried olde...
Does ST-Linux run for any configuration of eMMC pins, i.e. if it is connected to SDMMC1/SDMMC2/SDMMC3 . or do we need to fix as per reference design / Dev kits.
Hi Imen, Hi Patrick,Thanks for your valuable minutes. @Imen DAHMEN I'm using latest version which is 2.11.0. No issues with antivirus it worked for sometime & yes I tried restart and reinstalling several time after clearing disk. @PatrickF, Yeah I'...