STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Add new locale to image

I need to create an application that can handle text translations with gettext() in C code.How to add localizations to the image to be generated?I added these configurations in the build recipe:ENABLE_BINARY_LOCALE_GENERATION = "1"GLIBC_GENERATE_LOCA...

Using a U-Boot binary after building using the STM32MP1 Android distribution does not work.

Have tried building U-Boot with a few changes compared to the default ones using the STM32MP1 Android distribution.When changing the ssbl-trusted-fbemmc.img which contains the U-Boot binaries, the U-Boot start fails showing the following boot logs:/T...

SRaic.1 by Associate II
  • 1610 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP157F-DK2 Screen suspend issue

Than try to use this board with Debian Linux + Xorg happened strange behaviour: after one hour screen disabled forever. No any warnings or errors in dmesg. This issue reproduce on kernel from STLinux (5.15.67). Also these steps make same behaviour: e...

BVino.1 by Associate
  • 3458 Views
  • 2 replies
  • 1 kudos

Resolved! bitbake build errors

Hi All.I'm attempting to build an OpenSTLinux based software using a virtual machine VMWARE UBUNTU 16.2.5 build-20904516Using the command "bitbake -v -k <my_recipe_bb_name_file>" i have the error message: " ERROR: Nothing PROVIDES '–v' "Using the com...

nataut by Associate III
  • 1944 Views
  • 4 replies
  • 0 kudos