STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Kernel-5.15 bootloader dependency

Hi All!! I am currently using openstlinux-5.10-dunfell-mp1-21-11-17 for EV1. My idea is upgrade kernel version to 5.15 and keep u-boot-2020.10 and tf-a-2.4. My problem is that only upgrading the kernel and dtb, the kernel crashes and doesn't show any...

AVazquez by Associate III
  • 4222 Views
  • 6 replies
  • 0 kudos

Resolved! STM32MP1 - I2C frequency too low

In my device tree, we config 400KHz, but on scope we see only ~ 50Hz, and the clock seems weird. Anyone know why? &i2c1 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&i2c1_pins_a>; pinctrl-1 = <&i2c1_sleep_pins_a>; i2c-scl-rising-time-ns = <185>...

_legacyfs_online_stmicro_images_0693W00000bjEZXQA2.png
Dat Tran by Senior II
  • 2493 Views
  • 4 replies
  • 0 kudos

Resolved! STM32MP15x USART/UART Default Pins

Is stated on STM32MP157 datasheet's boot mode table that the MPU can be booted through UART: – USART2/3/6 and UART4/5/7/8 on default pins Nevertheless, I wasn't able to find which are the default pins for the UART interfaces, on the datasheet or refe...

Resolved! How to check, and eventually enforce Performance governor on STM32MP15 openst-linux?

I am trying to achieve hard real-time under 100us on the STM32MP157f-eval, specifically, on the Cortex A7 dual core.Note: I specifically target the Cortex A7 cores because the M4 is already taken for other tasks which requires much smaller latency.Wh...

A.M. by Associate III
  • 4701 Views
  • 7 replies
  • 0 kudos

HAL_SPI_Transmit times out

I have STM32CubeIDE Version: 1.12.0 and a STM32MP157F evaluation board.Created a M4 project and assigned SPI1 to it, generated the code.I then created a function to read a register:const uint16_t opcode = 0xe000; uint8_t value = 0; HAL_GPIO_WritePin(...

KBunn.1 by Associate II
  • 3132 Views
  • 6 replies
  • 0 kudos