STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Crypto Lib on STM32L051C8

Hello,I'm trying to integrate latest crypto lib (v. 3.1.2, FW implementation) into my TrueSTUDIO project but encryption with AES-CBC-128 fails.Example project in Fw_Crypto\STM32L0\Projects\STM32L053R8-Nucleo\AES\AES192_CBC fails both encryption and d...

STM32L4: Read Out Protection Level

Hi, I use STM32L431CCT6 for development.Occasionally, even I have no done any special operation, read out protection mode is enabled.(Level0→Level1)I do not know the cause clearly.Please tell me the cause or ​reproduction method.And is there any solu...

TNaka.0 by Associate
  • 1711 Views
  • 3 replies
  • 0 kudos

Bug in HAL_CRC Module

I found a bug the HAL CRC Module... First of all... when you enable the CRC Module with CubeMX 5.0.1 the MX_CRC_Init() is empty and the peripheral is not initalized!I wrote all the code manualy or copied it from the old CubeMX 4 generated code...This...

CRC module init code

Is STM32CubeMX v5.01 supoosed to generate CRC intializtion code? All I get is an empty  MX_CRC_Init() function and no handle is created. Is this a bug? I can copy the init code from an example but I'm wondering how/where the CRC clock gets enabled...

Firmware Encryption AES-256

Hi,I need to add the security and encryption to my firmware for the STM32L432KB MCU.Please suggest me that how do It or develop it.Thanks

K_P_D by Associate II
  • 1956 Views
  • 3 replies
  • 0 kudos

x-cube-cryptolib with cubemx

The question has been asked already, and the answer is generally : look at https://community.st.com/docs/DOC-1557-one-way-to-use-the-x-cube-cryptolib-with-cubemx-and-system-workbenchUnfortunatly, the link is dead.Where can I find this document ?Regar...

STM32 Cryptographic Library

Hello, I am using STM32 Cryptographic Library. as the UM, there are 8 .lib file. what is the difference? e.g M3_CryptoFW_RngHW_2_0_6. lib, is it implemented by Hardware? Or what crypto function is implemented by Hardware? does it include all crypto...

sliu.8 by Associate
  • 1455 Views
  • 2 replies
  • 0 kudos