STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Optimizing X-CUBE-CRYPTOLIB for memory constraint

Hello!I want to use Asymmetric Crypto algorithms like ECC or RSA for my FreeRTOS project running on STM32F051K8. The controller has 64 KB of flash. Since X-CUBE-CRYPTOLIB occupies quite large memory footprint, my FLASH is getting overflowed by the .t...

0690X00000AQxHwQAL.png
kvkhekale by Associate II
  • 1193 Views
  • 1 replies
  • 0 kudos

Setup CRC via STM32CubeIDE 1.02

I am trying to set up the CRC in an STM32L072 to process data from a 1-wire device.In the CubeIDE (editing the .ioc file), if I leave the default values, it will generate an appropriate MX_CRC_Init(void) function.But if I want to set my own polynomia...

Can't reset RDP from level 1 to level 0; Nucleo L476RG

Hi,I was testing with the Nucleo STM32L476RG board, BSP example project FLASH_DualBoot.I made small changes in the example code (LED blink stuff) and programmed bank 1 and 2 several times. I also manually checked/toggled the option bytes BFB2 bit a f...

Resolved! An issue in finding appropriate MCU to drive application.

We are developing an application where the host controller will drive two radio modules.But Host controller software should have MISRA 2012 compliant SDK with RTOS support and should support FIPS-certified crypto library.Do anyone can help us to find...

FM_360 by Associate II
  • 1517 Views
  • 3 replies
  • 0 kudos

STM32f42xx CRC stop/resume

HelloSince the STM32f42xx series has no intial value for the CRC I'm wondering if there is a way to stop a crc calculation (store the DR value) and resume it by writing the DR register with the stored value and some calculation??Something like this:c...

stucmath by Associate II
  • 7954 Views
  • 17 replies
  • 0 kudos