Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I ran into some problems with the E-L9826 low side driver.

Here is my hardware design. The output with load goes high during chip reset. When I cancel the reset, the output immediately goes low before I have done any control. I turn the output on or off again with no effect and at this point the diagnostic d...

JC3_0-1746499575235.png
JC3 by Associate
  • 574 Views
  • 0 replies
  • 0 kudos

L9963E cell balancing

Hello.I have a problem with this IC. I can read cell voltages perfectly. but when I initiate cell balancing on selected cells, its not happening. for that I follow these steps:1- I enable cells by writing on 0X1C Register.2- I set UV threshold by wri...

Resolved! STWBC86 operating frequency

Does the charger IC ever operate outside of the specified TX FREQ MAX and TX FREQ MIN limits?For example, if the limits are set to 100kHz and 148kHz and the charger is operating at either limit, would FSK cause it to change the frequency below this v...

pEEter by Associate II
  • 792 Views
  • 1 replies
  • 1 kudos

Resolved! L7987 in LDO when VIN < VOUT programmed

HiI am working on an application with wide VIN from 6V-60V and the target VOUT is 15V 3A max.When VIN > 16V, L7987 should fit my application. Problem is that when VIN drops below 16V, eDesignSuite reports an error so simulation is not possible. It st...

KLeun1_0-1746423263144.png
KLeun.1 by Associate II
  • 2257 Views
  • 6 replies
  • 1 kudos

Resolved! Project files for Vienna rectifier and DC DC converter

Hello ST community,We are working on a 15kW Rectifier module for EV charging application. This module contains 15kW Vienna rectifier and 12kW DC DC converter, input voltage: 3 phase 415V, output voltage: 40V-120V. For this requirement, we are explori...

AkashG by Associate II
  • 887 Views
  • 1 replies
  • 0 kudos

3.3KVA Single phase non isolated solar on grid Inverter

Hello ST Team, Greeting from Uniglobus, is the child R&D Electronics company of Polycab India limited My self Grishma Bhatt, I am Power Electronics Design Engineer We would like to start a new product 3.3KVA Single phase non isolated solar on grid In...

Grishma1 by Associate II
  • 2013 Views
  • 5 replies
  • 0 kudos

Resolved! STEVAL-10MLPVCB Code

Hi,I am building a 3L Buck Converter with MPPT tracking, using the STM32G474CBT6.The STEVAL-10MLPVCB has a very similar concept to what I want to achieve, I based my MCU choice and other details on it.Is it possible to obtain the source code / CubeID...

janik by Associate II
  • 1069 Views
  • 1 replies
  • 0 kudos

L9825 SPI INTERFACE TIMING related concerns

I have following three concerns related to SPI interface timing of L9825 low side driver IC. Please refer the image below. 1. Do we really need to toggle the clock signal within 100ns after NCS changed from High to low. If this 100ns is exceeded what...

Query.png
Deva by Associate
  • 945 Views
  • 1 replies
  • 0 kudos