Skip to main content
Chetna
Visitor II
October 7, 2024
Question

STEVAL-PMIC1K1

  • October 7, 2024
  • 1 reply
  • 657 views

Hi,

Can I get the schematic of STEVAL-USBSTICK which is part of the set STEVAL-PMIC1K1 and acts as an USB-I2C interface, to get the details of the CN1 connector & the other pin details.

 

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
October 12, 2024

Welcome @Chetna, to the community!

The STEVAL-USBSTICK is a proprietary tool, so schematics and other documents are not publicly available. It only works as a simple USB-I2C interface, as also mentioned in AN5440.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.