Question
AC?DC conversion system
Dear all
I would like design a circuit for AC/DC conversion of a 3 phase AC voltage with different frequency and different amplitude. The input power of the circuit can be changed form 4W up to 300W. Actually, circuit input is generated by a output of a 3 phase generator which is linked to a small wind turbine, so its frequency and output voltage varies considerably. Maximum output voltage is about 36v.
I appreciate it if you instruct me for using the ST parts (power modules) similar to VIPER31.
Best regards
Amin