Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I have a USB-C Power Delivery source with a receptacle (no captive cable) . The output of the switching mode power supply and the USB-C receptacle must be separated by a switch due to the cold socket principle of USB-C.Is a single FET sufficient or a...
now we have following situation.the circuit works fine at using the BTA16at using the T1635H-6T the hase cutting doesn't works ( full wave is engaged over the PWM range )Questions:a. what is the difference between T1635 and T1635H-6T ?b.how can we so...
I am designing a typical TRIAC drive circuit, opto drive of the gate, snubber, transient protection etc. All app notes I read are saying that the load to be driven (in my case the primary side of a transformer) should be placed on the TRIAC's MT2 pin...
I have created a .sfc file which I successfully write to my stepper motor. I need to drive the motor in Full step mode (which I am doing at present). Stepper motor is a 1.8deg motor - so 200 steps per complete revolution.
So I have some tiny stepper motors I've been working with. Very small 8mm tall x 7mm diameter and coil resistance is 40 ohm. We're designing some tiny digitally controlled dial gages around these and wanted to direct drive the needles instead of tiny...
Having problem on driving a motor with L6470 at speed range around 120 - 300pps where motor vibrates and making buzzing noise ,especially louder at 150 step/s, or mounting on a panel where the whole mechanical piece parts is vibrating together.Alread...
Please explain the purpose of 4 Parallel MOSFET, Why we cant use 1 or 2 MOSFET with higher rating, Also Why three seperate MOSFET driver is used for each phases, Why single Driver with 3 Channel is not used. Whether it can be used, Please suggest any...
Hi. I would like to know if it is possible to use Ihm08m1 to drive bldc with 3 independent Pwm...to not use complementary channels ? If so, is there an example how to drive l6398 correctly ?