User Activity

Hi,I am getting started with VL53L4CD so as to improve our system under ambient daylight conditions, which is performing poorly due to current sensor VL6180x under such condditions.My application is:Waking up device when target detected closer than 1...
Hello,I am trying some settings on VL6180x for avoing "Max_Signal_To_Noise_Ratio" when ranginf under sunlight conditions.I have tried to disable DMAX (#define DEF_DMAX_ENABLE     0), but still I get the MAX snr errror.I have been trying to set other ...
Hello,I am experimenting some trouble when using sensor VL6180X outdoors due to sunlight.The lasers are continuously seeing a yellow surface at 15cm. I get good rangings under Indoor light condition.The point is the lasers do not see any backgound w...
Hello,I have been requested to have our RFID reader compatible with Android, iOS and physical cards.Android can perform HCE and NDEF messages can be read with our current reader (ST25R95). So far, so good.But, it seems apple is forcing to use Apple V...
Hello,I am trying to read data from iOS/Andriod App with my reader.Currently, my reader is based on st25r95 and it is in tag detector mode waiting for physical cards. Everthing is ok so far. Now I need to wakeup and get data from smartphone or pshysi...