Resolved! Is there source code available for STSW-ISB047FW
I am looking to change the functionality of the LEDs in this firmware. is there source code available for download?
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I am looking to change the functionality of the LEDs in this firmware. is there source code available for download?
Hi, the AN5114 describes in a good manner the isolated controll of a TRIAC. In chapter 3.3.1 there are some equations for determining the resistornetwork. But it seems that this equations do not really work for a ACST435 with 35mA gate current and fo...
Hi. There is a question about "L78L05ABUTR" regulators. It's marking code is shown as "8C" in catalogue. But, It's actual product marking code is "8C033" (We bought "L78L05ABUTR" from Digi-Key.) I am curious what is right.
See AN436. I am using T1635-6G in a Hybrid Relay configuration following AN4993. Load is about 2kW at 230 VAC. Circuit works fine at with gate traiin of pulses (2kHz, DC = 50%). I want to trim parameters to optimum, at the moment transformer is make ...
The customer expected the full part-number as marking..We pointed him to the mfr label which shows the correct part-number and the marking.The hint in the datasheet showing that the marking is limited to 7characters with the last 2chars of the P/N be...
I have a STEVAL-SPIN3202 board and I have a linear stage (2-poles, 3 phases). To prevent collision with the endings of the stage, there are connected two end-stops. (One on both ends).Is it possible to use the STEVAL-SPIN3202 board for this setup? Or...
https://www.amazon.it/DealMux-Motoriduttore-encoder-Rapporto-trasmissione/dp/B07Y72T5BJ?pd_rd_w=hZaC3&pf_rd_p=b928db63-55ee-49e1-8ca9-807c91a11a4c&pf_rd_r=FMAZFZZ865BW326H55X9&pd_rd_r=c08f27cc-b043-4ac6-bd73-a3924ed21699&pd_rd_wg=8qSBw&pd_rd_i=B07Y72...