cancel
Showing results for 
Search instead for 
Did you mean: 

I'm using SPV1050 for charging with 18650 batt with 12V Voc panel 280mA, 2.8W.. Would want to know whats the max. input current the IC can withstand..

AK H
Associate II

I'm using SPV1050 for charging with 18650 batt with 12V Voc panel 280mA, 2.8W.. Would want to know whats the max. input current the IC can withstand.. Config settings are R1-10M, R2-1M, R3-5.6M & R4-6.2M, R5-500K, R6-2.7M.. Output current is limiting to 2.5mA at approx. 70000 lx(sunlight) value.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0