Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

the address of stc3100

Bits DevADDR0 to DevADDR2 are factory-programmable, the default device address valuebeing 70h (AddrID0 = AddrID1 = AddrID2 = 0).Can we change the address use DevADDR0 to DevADDR2?

Xniu.1 by Associate
  • 1338 Views
  • 2 replies
  • 0 kudos

stc3115

hii , we are using the STC3115AIJT to measure the SOC of the our litium-ion battery 4.2V 450mAH .i attached the drawing we have two problems 1- the voltage reg is correct but the SOC is alwayes 0 , we are using a full battery that we charged external...

Abeba.11 by Associate II
  • 1342 Views
  • 0 replies
  • 0 kudos

Resolved! LD39200PU33R

Hi, recently we purchased LD39200PU33R Fixed voltage circuit.i have to give 5v input voltage but i get 4.7V..that datasheet mentioned 3.3V..expected voltage i didn't get..

Resolved! When will VNH3SP30TR-E be produced?

I am an employee of Tata Daewoo Commercial Vehicle in Korea.I'm a member of the purchasing team, and I'm in charge of Tyco AMP.BCM, which is supplied from Tyco AMP, needs your VNH3SP30TR-E material.However, we are not receiving supplies from your sup...

Bkim.51 by Associate
  • 1292 Views
  • 3 replies
  • 0 kudos