STWBC GUI with STEVAL-ISB045V1 firmware download
i bought STEVAL-ISB045V1, so i should download firmware STEVAL-ISB045V1_QI_2.5W_V5.241.but if i do Setup-Load FW to board then Download error.I matching COM port though.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
i bought STEVAL-ISB045V1, so i should download firmware STEVAL-ISB045V1_QI_2.5W_V5.241.but if i do Setup-Load FW to board then Download error.I matching COM port though.
Please, Help me identify it and are there any analogues?
I refer to two (2) devices used for control of LLC DC-DC converter: L6599, and the newer L6699.In our application, we must enable and disable the gate drive output pulses via a separate signal. The transition from ENABLE to DISABLE must be instantan...
The datasheets states a device package of SOT23-5L. It states a pitch of 0.95 mm. However, when I downloaded the LDK220 SOT23-5L step file, the measured pitch is 0.65 mm. So, before I incorporate this device into my design, can someone please clar...
I was using the STEVAL-IPM15B board to generate a single phase output between the U and V phases on a 24 ohms resistor load. Thus, I was also using only 2 pairs of IGBTs (A and B) out of the 3 available. Everything that was connected to the W phase ...
Hi,We are using STEVAL-ISB68WA EVMs to validate Qi based wireless charging functionality for one of our application. It looks like our Qi standard transmitter is not able to detect the ISB68WA receiver, when tried placing on the top of the transmitte...
Hi, I am trying to program the evaluation board (I2C) without the NUCLEO board or GUI. I have configured the power profile correctly for PDO3, and confirmed through a register read on RDO_REG_STATUS, but the board keeps capping the power output at 20...
The VIP ER06XS is up to 800V.The T1 is need to endure 600V.The D28 STTH1L06A is up to 600V.The STGD6M65DF2 IGBTs power stage featuring:– V(BR)CES = 650 VThe STSPIN32F0601 is up to 600V.
Hai, I wanted to make a battery charger using non isolated boost IC. I came across this TSM Voltage and current controller IC. But this IC has been only used in insolated application. Is it possible to use this IC in non isolated converter. I w...
Hi. I am using an STM32L073 based nucleo board. There are 2 external wakeup pins configured on PA0 and PC13 in this board which can be used to wake the device out of standby. If I write code to configure these two wake up Pins to wake up from the sta...