cancel
Showing results for 
Search instead for 
Did you mean: 

Is the X-NUCLEO-IHM08M1 inverter compatible with any STM32 NUCLEO board?

SGada.1
Associate

Is the X-NUCLEO-IHM08M1 inverter compatible with any STM32 NUCLEO board?

Or is it only compatible with NUCLEO-F302R8 NUCLEO-F401RE?

In all the documentation I have seen it is used only with these boards. I need a better board such as the NUCLEO-H743ZI for my application. Before buying the parts I wanted to confirm if the X-NUCLEO-IHM08M1work with any STM32 NUCLEO board.

PS : When I say work with I mean, will it sit on the board correctly with the proper pins in the right place. Such as ADC pins of the MCU on the current sensing pins of the inverter.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0