VNH5050 diag pins and pwm input
I am designing a quad motor controller using 4 vnh5050. The motors will be controlled independently through INA1 - INA4 & INB1 and INB4 signals from uC.
In order to keep pin count usage down:
1) Can I connect the DIAGA and A DIAGB pins together and just have 1 fault pin going to uC from each vnh5050? (if there is a fault in either I will try to reset both)
2a) Can I run the same PWM signal to all 4 vnh5050's? ( I will generate a constant PWM signal of desired motor speed connected to each vnh5050 and using the INAx and INBx pins for the desired vnh5050, turn the motor on/off.)
2b) Can the PWM remain HIGH for full speed or does it require PWM?