Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is T1620T-8I on OK alternate to BTA16-600BRG

I have a circuit very similar to AN4993 figure 7 that used a BTA16 Triac. They have become hard to find, so I am looking at replacing it with the more modern T1620T-8I , which is a snubberless triac. After reading AN4993 several times, I just want to...

0693W00000QL2NNQA1.png 0693W00000QL2PiQAL.png

I am using L6470 in my project and I have a serious problem. the voltage / frequency profile is corrupted for no apparent reason.

After the initial setup I only use two commands HARD-HIz and RUN. I'm interested in the speed of the engine.Everything seems to work fine, but if I update the speed setpoint repeatedly with values very close to each other gradually the current suppli...

Lorenzo1 by Associate II
  • 661 Views
  • 0 replies
  • 0 kudos

Resolved! STLQ020PUR output discharge function

Hello,I am interesting in STLQ020PUR WITHOUT the output discharge function (presented as an option) : there is no information in the datasheet to recognize if this option is present or not versus the device reference STLQ020PUR : how to be sure ...

LGARC.1 by Associate
  • 999 Views
  • 3 replies
  • 0 kudos

Power Converter Firmware Design

Hey, can anyone suggest any App-Notes/ Guides/Resources for designing AC-DC/DC-DC Power converter Firmware, such that if we use two or more modules in Parallel and they sync with each other so that we can have a modular system (we add/subtract no. of...

Geetansh by Associate II
  • 1011 Views
  • 0 replies
  • 0 kudos