User Activity

I want to use my ST25DV with both I2C and RF interfaces. There is no clear arbitrage between the 2,  but the first is served. Moreover, I tested that while I2C is operating in reading and writing bytes in a for loop, the RF can corrupt the data in so...
I am using a PN7150 with ISO 15693, and the resulting sequence is :0x00,0x00,0x07, 0x21, 0x30, 0xB6, 0x1D, 0x00, 0xB2, 0x00first 3 bytes written on the nxpNci level, then my message. I want to read some blocks, in particular I would like to read all ...
I bought a STWBC2-HP and I designed a board as specified in the datasheet, but I can't find any support for the firmware part. Do you have any block code to integrate to a custom firmware to drive the mosfet and implement the WPC protocol?
Kudos given to