Skip to main content
Md Mubdiul Hasan
Associate III
November 18, 2021
Question

Low cost DC-DC converter/SMPS design idea and suitable topologies

  • November 18, 2021
  • 0 replies
  • 668 views

Hi there,

I am looking for a customized design where good power solution can be applicable.

My aim is to develop a DC-DC sutable toloplogy ( flyback, buck, isolated ,..so on) converter with following parameter, with the idea https://www.smps.us/topologies.html

INPUT: 250 to 650 VDC

OUTPUT: 24V/5A , 5V/3A, 12V/2A.

Lets think its saparate system for all output. Offcourse this design is challenging since it has wide range of input.

 Its for battery charger or EV application.

This topic has been closed for replies.