Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bring-Up of L6591 without PFC

 Hello everyone,we are currently trying to bring up the L6591 without PFC, but unfortunately we have not been successful so far.It looks like the L6591 is not able to start up correctly.The Vcc voltage slowly rises to about 14V with the built-in HV s...

camillem by Associate
  • 348 Views
  • 0 replies
  • 0 kudos

Resolved! Thermal Resistance of the SOT-223 Package

I am selecting the LD1117S50CTR. The package is SOT-223.I understand that the thermal resistance Rthja = 110 °C/W shown in the datasheet is the value for the IC alone.Since I am designing the PCB, I would like to know the relationship between copper ...

Matsuura by Associate II
  • 865 Views
  • 4 replies
  • 1 kudos

PowerSTEP01 Low speed optimization

I cannot see the effect of the low speed optimization.I set speed to 1 rpm and watch the phase currents.With these settings (these values are readbacks):min_speed: 0x1fdfconfig: 0x2c90step_mode: 0x0007I get significant distortion around 0 A:To compar...

Gostervall_0-1763385262693.png Gostervall_1-1763385324820.png

PowerSTEP01 self-contradicting datasheet

The PowerSTEP01's datasheet says on page 34 that MIN_SPEED is 12 bits wide.On page 37, it is described as 13 bits wide.I suppose that 13 is correct, from code I've read online, but a confirmation (and fix) would be nice. I cannot see the low speed op...

Test result data for 5V output device LDK220U50R

Hello Team,We have selected part no: LDK220 and LDK320 with a SOT-89 footprint for one of our applications. We have referred to the complete datasheet, but we have not found the test results for 5V output category devices, like the voltage dropout of...

JYada.1 by Associate II
  • 470 Views
  • 3 replies
  • 0 kudos

STEVAL-ISD01KCB

I've been looking at the STEVAL-ISD01KCB, and I saw in an image that it has some capacitors between pins 8 (-DC) and 9 (+DC). What is the value of that capacitor? Is it necessary to include it? I ask because I've noticed that this capacitor slightly ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.