Where can I find the source code for the firmware on the STEVAL-WLC38RX and STEVAL-WBC86TX boards? I'd like to start there and make some modifications.Thanks.
I get an error message when I try to connect with the STEVAL-WLC38RX evaluation board using STSW-WPSTUDIO. I am using v2.7.2 of WP Studio. See error message attached.
I want the Tx and Rx to communicate with each other to confirm they are both products from my company before charging. I don't want the Tx to charge a device if it is not from my company, and I don't want the Rx to charge with any generic Qi device.
I am still struggling with mine as well, however I did get past that screen when attempting to connect to the WLC38 eval board. The part I missed was Step 2 in the picture below (also find it at the link here). If you have a Qi transmitter Step 2a ...