cancel
Showing results for 
Search instead for 
Did you mean: 

3.3KVA Single phase non isolated solar on grid Inverter

Grishma1
Associate II

Hello ST Team,

Greeting from Uniglobus, is the child R&D Electronics company of Polycab India limited
My self Grishma Bhatt, I am Power Electronics Design Engineer
We would like to start a new product 3.3KVA Single phase non isolated solar on grid Inverter
I am looking for a solution from ST. Whether will get Evaluation Board?
Will get Hardware and firmware support?
 
I am sharing technical specification for a detail
5 REPLIES 5
Peter BENSCH
ST Employee

Welcome @Grishma1, to the community!

Your inverter must surely also have MPPT because of the solar feed, right?

Such applications are always application-specific, so there is no ready-made evaluation board available. However, your local distributor or your nearest office of STMicroelectronics will be happy to help you with a suggestion.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Grishma1
Associate II

Hello Peter,

Thanks for a response

Yes, Its MPPT based.

Could you please refer to Local Technical Team? 

 

You can find your local team using the link already mentioned by selecting the contact type ‚Distributors‘ and then your country.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

I have already tried with WPG and Future Electronics, But I got ans that ST will not support

I am not looking as complete EVM, I am looking for a collaboration.

Could you please refer?

I am Hardware design Engineer, and I have to develop with the help of ST.

Unfortunately I cannot help you with such High-Power applications, only the local distributor or the local office can.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.