STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to flash STM32H7B31 Code Menu Launcher

Hi Team I have tried flashing the Menu launcher codeI see that the device is not doing anything after flashing It gets halted while flashing I have attached the screen shot Follwing is the procedure that i followed Downloaded the code from the STM32C...

DRAME.1 by Associate II
  • 345 Views
  • 0 replies
  • 0 kudos

STM32H747 Dual Core Programming Both Cores

I have an application built in CubeIDE that utilizes both cores on the H747I-Disc1 board. The M4 core collects data and uses HSEM to notify the M7 core to process it. In debug mode I can run this just fine by first launching the M7, letting it run an...

RDock by Associate II
  • 1165 Views
  • 5 replies
  • 0 kudos

Program STM32 through bus CAN

Hello,Is it possible to program STM32* through bus CAN with STM32CubeProgrammer and STLINK-V3SET ?If yes :can we program only one STM32* even if many other STM32* are connected to the bus ?do we need to flash a bootloader or the embedded bootloader i...

Resolved! STM32H747 Discovery Kit Not Debug/Programmer

Hello;I can't program and debug with the STM32H747 Discovery kit. I tried Stm32cubeProgrammer and STM32CubeIDE for this. Below are the errors I have received in both.Debug configuration screen is below;STLink Serial number appears, but I can't unders...

0690X00000AsYXWQA3.png 0690X00000AsYXgQAN.png 0690X00000AsYXqQAN.png

CubeIDE External Loader

Hi everyone,We're using G474 is new MCU and want to program an external flash via STM32CubeProgrammer. However, IDE can't generate valid stldr file or I have done wrong its settings. I have set the parameters as example for atollic. CubeProgrammer do...