STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Shutting down... Exit.

 STMicroelectronics ST-LINK GDB server. Version 7.7.0Copyright (c) 2024, STMicroelectronics. All rights reserved. Starting server with the following options:Persistent Mode : DisabledLogging Level : 1Listen Port Number : 61234Status Refresh Delay : 1...

asda by Associate
  • 2263 Views
  • 1 replies
  • 1 kudos

bank mode and data alignement

Hello,I'm currently working with the STM32G474RE microcontroller and aiming to transition from the standard dual bank mode to the single bank mode.However, I've encountered an issue during this transition. When switching the bank mode, the read width...

Unbenannt.PNG
ssmrabhi by Associate
  • 1783 Views
  • 3 replies
  • 0 kudos

Command line interface -w32 and -w64

Hi.I wanted to know if the -w32 command always performs a sector erase?Does the -w64 command always perform a sector erase? If they always delete the sector, is there a command that doesn't do it?Best regardsJk 

IHS1 by Associate II
  • 1195 Views
  • 1 replies
  • 0 kudos

Resolved! Command Line Interface

Hi Everyone,I want to know Is any possible way available so I can upload firmware for my custom stm32 board using Command Line Interface? ST providing any Command Line Interface and commands?Unfortunately, I could not find ST Cube Programmer CLI. I c...