STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32WB10CC not programming on custom hardware

I designed a custom PCB. It is designed to be used in a remote control car I want to make/to control a BLDC motor and servo wirelessly or through a potentiometer.When I attempt to program the microcontroller (connecting through STLINKV3) it seems to ...

nmartini_0-1716614990108.png
nmartini by Associate II
  • 4768 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 ST-Link Utility not working?

So i installed the st-link utility from my.st.com and did all the installation but when i run it, it tells me there are some .dll files missing. Specifically, these are the errors; 1st error; "The code execution cannot proceed because mfc140.dll was ...

Resolved! SFI with HSM license

Hi,I want to install an SFI on my microcontroller (NUCLEO-U575ZI-Q) using the following script:#!/bin/sh# Set to the default installation path of the Cube Programmer tool# If you installed it in another location, please update pathtool_dir=~/STMicroe...

licencia_hsm_3.png
mikel-m by Associate III
  • 1505 Views
  • 1 replies
  • 0 kudos

STM32429I-EVAL1 Touchscreen does not work

HelloI'm using STM32429I-EVAL1 and its touchscreen is not working.When I plug st-link cable, originally touchscreen was initialized and displayed menu.But now, it only displays totally white screen and there is no reaction when I touch it.I did Softw...

Unlimit by Associate II
  • 1498 Views
  • 2 replies
  • 0 kudos

Resolved! Error connecting with ST-LINK in Linux

Hello,I have installed STM32CubeProgrammer (version 2.14.0) on a Linux machine. I have connected my NUCLEO-U575ZI-Q microcontroller to the machine, but the CubeProgrammer does not detect it (the machine does). I received this message on the CubeProgr...

mikel-m by Associate III
  • 4741 Views
  • 1 replies
  • 0 kudos