2023-10-20 7:25 PM
"DCMI_SnapshotMode DCMI Snapshot Mode example"
I am a beginner and would appreciate help with the following Readme.txt:
"In order to make the program work, you must do the following :
- Open your preferred toolchain
- For each target configuration (STM32H747I_DISCO_CM7 and STM32H747I_DISCO_CM4) :
- Rebuild all files
- Load images into target memory
- After loading the two images, you have to reset the board in order to boot (Cortex-M7) and CPU2 (Cortex-M4) at once.
- Run the example"
I hope the attached photo indicates that I have completed "Load images into target memory".
How do I complete the remaining steps?
2023-10-20 8:47 PM
Power cycling the board (remove power, then re-apply power) will cause it to start whatever program you have loaded on there.
2023-10-22 12:41 PM
Have I loaded the dual core programs correctly? Please view the photo.
2023-11-01 3:53 AM - edited 2023-11-01 4:05 AM
Hello @kevin-gordon and welcome to the Community :),
Besides, the reply shared by @TDK, note that STM32H747I-Disco have many revisions boards. So, which MB1166 Rev.A are you using? A01, A03...?
If you use MB1166 Rev.A03 or A09 please try this fix on GitHub :
You just need to enable the right hardware component as defined in stm32h747i_discovery_conf.h file and add the new component library (NT35510) in your project .
/* IMPORTANT: One of the following flags must be enabled in stm32h747i_discovery_conf.h file */
/* options in order to select the target daughter board revision connected on STM32H747I DISCOVERY : !!!!!!!!!! */
/* USE_LCD_CTRL_OTM8009A */ /* Applicable for all LCD daughter boards (MB1166) except for Rev -A09,-A03 */
/* USE_LCD_CTRL_NT35510 */ /* Applicable only for LCD daughter boards (MB1166) Rev -A09,-A03 */
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.