STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

.dfu files do not work after download

Hi,I'm using the STM32CubeProgrammer to program an STM105. I connect it via USB (in boot mode) and I can connect successfully. Downloading a .dfu file for the project works as well.However, after everything is complete and I unplug and reconnect the ...

MarcoP by Associate
  • 1931 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 programming via USB

I am programming USB DFU in stm32f407g disc1 but i am not able to connect it in stm32cubeprogrammer as it is showing usb port as usb1. Can anyone tell me is it anything missing?

Uninstalling STM32CubeProgrammer on Linux

Hello,There have been several similar threads but no answer from ST:https://community.st.com/t5/stm32cubeprogrammer-mcus/uninstall-stm32cubeprogrammer-ubuntu/td-p/335445https://community.st.com/t5/stm32cubeprogrammer-mcus/how-to-uninstall-stm32cubepr...

sute by Associate III
  • 1930 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CUBE Programmer development is not complete!

Instead of completing development of STM32CUBE Programmer - every one now need to follow some manual steps with unknown versions of firmware with many undefined startup addresses and even when all steps are completed with success - development board ...

GS2 by Senior II
  • 6741 Views
  • 15 replies
  • 5 kudos

Read from motor controllet vio

OK so total noob here with a issue, I am trying to read from an esc/motor controller  through jtag ,problem lies in the fact  that iim using St link and bluepill  and there connected throigh  sclk sdio c9nnections.so my question is how and what to do...