STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32CubeProgrammer Java version

We are trying to use STM32CubeProgrammer on Windows computers running JDK 11 and higher. Is this not supported by CubeProgrammer? It does not appear that the program contains the typical BIN file that we would edit to use a different version of Java ...

jw56 by Associate III
  • 1726 Views
  • 1 replies
  • 0 kudos

I used STM32CubeProgrammer v2.1.0 in utuntu 18.04. Connect STM32F103ZET6 failed. Usb to serial port is WCH CH340G.

13:05:04 : Serial Port ttyUSB0 is successfully opened.13:05:04 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off13:05:05 : Timeout error occured while waiting for acknowledgement.13:05:05 : Timeo...

ljing.17 by Associate
  • 833 Views
  • 0 replies
  • 0 kudos

Cannnot start STM32CubeProgrammer.app

I just installed STM32CubeProgrammer on my Mac running MacOS Mojave with Java 8 installed. Everything installs OK. But I cannot run the app. I have tried Show Contents on the .app file and run /Applications/STMicroelectronics/STM32Cube/STM32CubePr...

spdaly by Associate II
  • 695 Views
  • 0 replies
  • 0 kudos

I'm trying to program a stm32l031k6 MCU using the UART interface and cube programmer.

BOOT0 is high and the chip is reset. Using the following command:./STM32_Programmer_CLI -c port=/dev/ttyUSB0 -vb 3 -ob displi'm getting the following result:     -------------------------------------------------------------------                     ...

Fabry by Associate
  • 1585 Views
  • 2 replies
  • 0 kudos

STM32 Cube Programmer API

Besides function "downloadFile", is there a way of program flash using a buffer ?The use case is not to have a firmware file, protecting the programming phase on third parties (assembly lines, testing).

rbenv.3 by Associate II
  • 1302 Views
  • 2 replies
  • 0 kudos

How can I program STM32L011 prototype board

Hello all,I am using STM32L011K6_Nucleo Board for developing a smart application, now I making prototype with STM32L011 microcontroller and some other sensors. My doubt how should I program my prototype board? what are the connection do I have to lea...

VDhan by Associate II
  • 2224 Views
  • 3 replies
  • 0 kudos