STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP2 disable CPU_IDLE on Linux

 Hi,I am debugging the STM32MP257F-EV1 board with a debugger via JTAG/SWD. The kernel version is 6.1.82.To provide complete debug access and to prevent the JTAG/SWD from shutting down when the CPU is idle, I think [CONFIG_CPU_IDLE] has to be disabled...

Aiyps by Associate II
  • 1831 Views
  • 0 replies
  • 0 kudos

Resolved! OpenSTLinux - wxWidgets

Hi!Will/Can OpenSTLinux run/support C++ applications that are made with wxWidgets? If not: Can ST Dev team implement it? wxWidgets is using GTK native widgets on linux. GTK is written in C.I recently found that wxWidgets isin't so bad after all, comp...

DMårt by Lead
  • 2168 Views
  • 4 replies
  • 3 kudos

DDR3 RAM problem

Exception mode=0x00000016 at: 0x2ffebb4dNOTICE: CPU: STM32MP157DAC Rev.ZNOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery BoardINFO: PMIC version = 0x21INFO: Reset reason (0x15):INFO: Power-on Reset (rst_por)INFO: FCONF: Reading TB_FW firmw...