2023-07-16 10:53 AM
Hi all.
I'm developing a QT/QML application for my embedded openSTLinux project. This application has to play some videos with relative audio. I'm trying to play a mp4 file. If I use the following
gst-launch-1.0 playbin uri=file:///home/root/media/my_video.mp4 video-sink="waylandsink sync=false"audio and video are played correctly. Instead, if I use QML code, for example this
Item {
id: idVideo
visible: true
width: 1024
height: 600
Video {
id: videoExample
anchors.fill: parent
source: "file:///home/root/media/my_video.mp4"
autoPlay: true
focus: true
}
}or this
Item {
id: idVideo
visible: true
width: 1024
height: 600
MediaPlayer {
id: mdpExample
source: "file:///home/root/media/my_video.mp4"
autoPlay: true
}
VideoOutput {
id: videoExample
anchors.fill: parent
source: mdpExample
}
}the display shows nothing (black screen) but the audio is played correctly.
Below the "gstreamer" plugins I have installed in my openSTLinux image
gstreamer1.0 \
gstreamer1.0-plugins-good \
gstreamer1.0-plugins-base \
gstreamer1.0-plugins-bad \
gstreamer1.0-plugins-ugly \
gstreamer1.0-rtsp-server \
gstreamer1.0-omx \
gstreamer1.0-libav \
gstreamer1.0-dev \
gst-validate \
gst-examples \How can I solve the problem?
Thanks
Regards
2023-07-16 11:52 PM
Hello @nataut ,
I think your issue is related to the way you code your QML app to play the video.
I made a such kind of demonstration, and please see below the way I use Video Player:
MediaPlayer {
id: mediaPlayerVideos
source: "gst-pipeline: filesrc location=/home/weston/database/videos/" + video_src + " ! avidemux ! jpegdec ! qtvideosink"
autoLoad: false
autoPlay: false
loops: MediaPlayer.Infinite
// loops: 1 /* Play only once */
}
VideoOutput {
id: videosOutput
width : videoPlayer.width
height : videoPlayer.height * 0.8
opacity: 0.9
anchors.top: parent.top
source: mediaPlayerVideos
focus: true
visible: true
}
Of course, you will have to adapt the Gstreamer pipeline to your case, but what is important is to also use the "qtvideosink" at the end, to well integrate the video inside your Qt UI.
Please try to get inspire by this example and tell me your feedback if you can.
Kind regards,
Erwan.
2023-10-20 5:42 AM
Hello @Erwan SZYMANSKI ,
I'm sorry but I only noticed your response today
I tried your suggestion. I used the following pipelines
"gst-pipeline: filesrc location=/home/root/media/video_test.avi ! avidemux ! jpegdec ! qtvideosink"
"gst-pipeline: filesrc location=/home/root/media/video_test.avi ! decodebin name=dec ! videoconvert ! qtvideosink"
"gst-pipeline: filesrc location=/home/root/media/video_test.avi ! decodebin name=dec ! videoconvert ! waylandsink"
"gst-pipeline: filesrc location=/home/root/media/video_test.mp4 ! avidemux ! jpegdec ! qtvideosink"
"gst-pipeline: filesrc location=/home/root/media/video_test.mp4 ! decodebin name=dec ! videoconvert ! qtvideosink"
"gst-pipeline: filesrc location=/home/root/media/video_test.mp4 ! decodebin name=dec ! videoconvert ! waylandsink"but I have always the following error
Error: "No URI handler implemented for \"gst-pipeline\"."Thanks
Best regards
2023-10-20 5:49 AM
Hello @nataut ,
No problem for the delay, we know we had a little issue with mail notification and we apologize for that :)
Hmm I see. Which version of QtMultimedia do you import in your QML code ? In mine where things are working fine, I have followings imports :
import QtQuick 2.9
import QtQuick.Window 2.9
import QtQuick.Controls 2.9
import QtMultimedia 5.11
import QtQuick.Controls 1.4 as QQC1
import QtQuick.Controls.Styles 1.4If it changes nothing, can you tell me which OpenSTLinux do you use, and how did you generate your main SW image (Yocto, Starter image ?).
Rgs,
Erwan.
2023-10-20 6:11 AM
Hello @Erwan SZYMANSKI ,
I have the following import
import QtQuick 2.11
import QtQuick.Window 2.11
import QtQuick.Controls 2.4
import QtQuick.Layouts 1.11
import QtQuick.Controls 2.4 as Controls
import QtMultimedia 5.11I use a OpenSTLinux 4.19.94 version and it has been generated by means Yocto 2.6 version
Many thanks
Regards
2023-10-20 6:20 AM
@nataut ,
Can I ask you to do a test ? Can you turn the autoplay from true to false ? And then try to activate they play manually by another way ? This is just for test purpose, but I ask myself if I did not face something similar in the past, and if it was due to the fact that the play began too early in comparison with the media settings.
Rgs,
Erwan.
2023-10-20 6:35 AM
I tried the code below that generate the start/stop video touching any point of the screen
Item {
id: idVideo
visible: true
width: 1024
height: 600
MediaPlayer {
id: mdpExample
source: "gst-pipeline: filesrc location=/home/root/media/video_test.mp4 ! decodebin name=dec ! videoconvert ! waylandsink"
autoPlay: false
}
VideoOutput {
id: videoExample
anchors.fill: parent
source: mdpExample
}
MouseArea {
anchors.fill: parent
focus: true
onClicked:
{
if( mdpExample.playbackState === MediaPlayer.PlayingState ) {
mdpExample.pause()
}
else {
mdpExample.play()
}
}
}
}I have always the same error (the following)
GStreamer; Unable to pause - "gst-pipeline: filesrc location=/home/root/media/video_test.mp4 ! decodebin name=dec ! videoconvert ! waylandsink"
Error: "No URI handler implemented for \"gst-pipeline\"."
Many thanks
Regards
2023-10-20 6:39 AM
@nataut, As you are on an old baseline not supported anymore, I do not know what is fetched from Qt on the current one on which you are, and if the feature was already supported...
However, when I look at the version of Qt package you take, it does not make me feel we are far from each other. For now I do not have more idea, do you have the possibility to test on a recent distributition ?
Kind regards,
Erwan.
2023-10-20 7:01 AM
I have Qt Creator 4.8.2 based on Qt 5.12.1
At the moment I have no possibility to test on a recent distribution
Many thanks
Regards