Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PowerSTEP01 VDDIO Connection

Hi,We are using the chip PowerSTEP01 in our design. In the datasheet, it is mentioned in the application diagram that the VDDIO pin can be powered from the VREG pin. However, the X-NUCLEO IHM03A1 evaluation board design shows that it is powered exter...

bmkc by Associate
  • 1621 Views
  • 2 replies
  • 0 kudos

STP45N65M5 damaged

Hello. I am using your STP45N FETs in our power supply design for an audio amplifier and we are getting field returns with the STP45N65M5 part damaged. It appears that the gate and source have been shorted but I am not 100% sure. Do you have any insi...

arsaenz by Associate II
  • 12272 Views
  • 10 replies
  • 0 kudos

Resolved! L5970AD DCDC schematic doubt

Hello,I am investigating in using L5970AD DCDC converter for a 12VDC to 3V3 need.It was advised to me by the ST DCDC online simulator.It's a 20 year old circuit but it it matches the budget, the additional BOM and the efficiency so I am interested.Bu...

AlexMachine_0-1729210148466.png

unknown fault using STEVAL-L99615C

Hello,I have some questions regarding programming the development kit. We have configured a BMS IC and MCU using a 3-cell setup based on the development kit circuit. Our circuit replicates the schematic and pin configuration of the L99615, connecting...

JSleeeee_0-1730120588711.png JSleeeee_1-1730120595864.png
JSleeeee by Associate
  • 732 Views
  • 0 replies
  • 0 kudos

SPV1050 MPPT Resistor Setting

If you look at the SPV1050 constraints item in 6.4 MPPT Setting in the SPV1050 Datasheet, it is clearly stated that Vmpp(max) should not be applied over 2.1V.However, looking at an4397 (Application Note), even if Vin (Range: 2.6V ~ 9V) is more than 5...

Limiting DC current@110V to 2A

I am trying to design a current limiting circuit at 110vDC.(Range 90-140)Need to limit the current at 2A and provide short protection on the line.Is there any ST mosfets which can help acheive this requirement.Or I am wondering if there is any refere...

rishi2 by Associate III
  • 2240 Views
  • 4 replies
  • 0 kudos

Question on Gate driver VNQ860SPTR-E

I want to know about the compatibility check between the gate driver ic VNQ860SPTR-E and microcontroller PIC32MZ1024EFH144-I/PL  Can I use this gate driver for my above mentioned microcontroller.

Sau_rus by Associate II
  • 4970 Views
  • 9 replies
  • 1 kudos