Dear all,After converting the source code files from SPL to LL. I cannot see any project files in the destination folder. Can these source code files be used by either IAR or STM32cubeIDE? Or do I need to do some configuration first?Thank you.
Dear all, After the SPL2LL conversion, I got the messages below.Message 1: [WARNING] -- Line 2096 -- "NVIC_SetVectorTable" No LL API, StdPeriph legacy API is used instead (legacy library) Message 2:[WARNING] -- Line 238 -- "I2C_CheckEvent" No LL ...
Dear all,I am trying to convert the SPL to LL using the SPL2LL converter. After pressing the migrate button, I got the message below. Please help. Is it the problem that I chose the wrong directory? I chose the directory where the main.c file is loca...
Dear all,I am a BMS engineer looking for an automotive-grade BMS solution. Is L9961 good enough to develop an automotive-grade BMS for onboard battery pack monitoring? Do you have any other suggestions?Thank you very much.
Dear GS98, Thank you very much for your information.It seems that L9963E is a good solution. However, my application is for monitoring a single cell. We may not need the daisy chain function now, but an isolated interface is necessary. The voltage ra...
Dear Andrew, I am unfamiliar with the SPL2LL conversion and STM product, so I want to look for some hints here to shorten the development time. You are right! I trust all the answers can be found on the STM website and document. Thank you so much for...
Dear Andrew and Tesla, After the SPL2LL conversion, I got the messages below.Message 1: [WARNING] -- Line 2096 -- "NVIC_SetVectorTable" No LL API, StdPeriph legacy API is used instead (legacy library) Message 2:[WARNING] -- Line 238 -- "I2C_Check...