Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB PD Load Sharing

Hello, we are searching for a USB PD Power Budgeting/ Load Sharing solution. Here an example: Lets say we have 4 USBC PD Ports. All in all they sould be able to source 60W. One port is sourcing 15V/3A=45W, then the remaining 4 should just be able to ...

VH by Associate
  • 1175 Views
  • 1 replies
  • 1 kudos

Resolved! Voltage regulator to give 2.5V out from 3.3V in

I am designing an interface board where there is an ADC that needs two different power supplies (3.3V and 2.5V). To minimize this board, instead of bringing the two power supplies from outside, I would like to bring only the 3.3V one and through a vo...

Resolved! Calculate stepss for PowerSTEP01 (and L6480)

Hi, I am currently implementing software/firmware for the PowerSTEP01 chip and discovered a inconsistency in data sheet https://www.st.com/resource/en/datasheet/powerstep01.pdf. For parameter INT_SPEED (section 11.1.11 in datasheet) the equation does...

0690X000009k1YHQAY.jpg

Resolved! STSPIN32F0 Overcurrent detection R43 value

According to the reference circuit, R43 is 75kohm.Also UM2154 User manual said that R43 should be higher than 30kohm.What happens if R43 is 22kohm. Is overcurrent detected by STSPIN32F0?

0693W00000QMwylQAD.png
TYama.17 by Associate II
  • 4492 Views
  • 9 replies
  • 0 kudos

Diode IFSM estimation

HelloI need to estimate IFSM for certain current pulse.Does anyone know how to do it?I found this app note :Schottky diode avalanche performance in automotive applications (st.com)But it is not clear the method as intervals are weird :I ^4 x t = Cste...

Fausto2 by Associate II
  • 2177 Views
  • 3 replies
  • 0 kudos

Resolved! POWERSTEP01 : sense resistor

Regarding the shunt resistors connected to the SENSEA and SENSEB pins, the UM1829 has three 0.1 ohm resistors connected. Why is this? The datasheet says one 0.1 ohm resistor.Do I really need three of them?

naoki by Associate
  • 1140 Views
  • 2 replies
  • 1 kudos

Resolved! Can STUSB4710 act as a DRD?

Hi, Can PD Controller (STUSB4710) act as a DRD?STUSB4710 - Stand-alone USB PD controller (with short-to-VBUS protection) - STMicroelectronicsI believe that STUSB4710 cannnot operate as DRD (Dual Role Data), and can only function as UFP.If there is a ...

MMSK by Associate
  • 1393 Views
  • 2 replies
  • 2 kudos

Resolved! VNQ9025AJ Output pin Current capacity

Hey, probably a dumb question, but I couldn’t find it in the datasheet. Can each pin of the VNQ9025AJ handle 30A, or is that the rating for the smart switch as a whole with a limit on each pin? Honestly, I’m hesitant to believe a single pin can handl...

Resolved! VIPer22A Isolated DC-DC Converter

Hi,When I was trying for DC-DC converter design, I have found this VIPer22A Isolated DC-DC converter design. I am having two queries here,1) Is still this technology in use?2) Can I get the details about the transformer which used here?Is there any n...

Shangugapriya_G_0-1730266992697.png