Resolved! MSL of part#STP85N3LH5
Please review and advise what is MSL(Moisture Sensitivity Level) of part#STP85N3LH5. We are aware that this part is "obsolete".Please provide a related link /document showing the MSL of this part.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Please review and advise what is MSL(Moisture Sensitivity Level) of part#STP85N3LH5. We are aware that this part is "obsolete".Please provide a related link /document showing the MSL of this part.
Hi! I'm new in this forum, and my english is not the best, but I will try to explain myself. I'm charging Lead-Acid batteries with a transformer, and a bridge rectifier. If there was no battery, the signal will be a pulsating signal, but because the...
Dear support team, can I run both outputs of the VND5004ATR-E parallel to decrease the RDSon even more? So just connect both inputs and the load on both outputs? Thanks
Dear STM Team,Please answer to my below queries:1. Can you please let me know the maximum frequency can be provided to IPS1025HTR-32 and VN750PSTR-E to enable or drive high side switch?2. Can we drive these switches at lower duty cycle up to 1%? Rega...
Hey ST community!I am trying to download the GUI for the STEVAL-L99615C from this LINKBut when I try to unzip this folder I get an error saying that the file is invalid. Is this happening to anyone else?Thanks for any help!
Good morning sir Pls identify the component.i don't understand
Hi everyone,I’m designing a 3-phase SMPS using the VIPER22A and need some assistance with the transformer design. Below are the key design parameters:Design Parameters:Input Voltage: 150 VAC to 420 VAC (50 Hz)Output Voltage: 5.5 V DC, 2 APower Output...
Hello ST Microelectronics Community, i need your Help. Which Part Marking has LD1117DT33CTR TO-252-3, DPAK ? Yours sincerly Badis Gara
What is the recommended RLIM value for Vout of 28V and Iout of 60mA?
Im planning to use the LDO LD39015M12R with 1.8V Vin, VOut=1.2V 5mA load current. the drop out voltage is 80mV but the datasheet shows the condition of Vin= Vout+1v in the electrical characteristics table.My case will not meet this Vin=Vout+1V condi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.