User Activity

I want to get the LTspice model corresponding to the fluorescent light ballast controller L6574, I have searched all kinds of information on the Internet, but I did not see the information I want, can someone help me? Thank you very much:grinning_fac...
I have the following questions and need help:1. Can this transistor be used at a frequency of 900kHz? Can it only be used in frequency bands above 1MHz?2. The data sheet provides a test circuit under 30MHz conditions. We do not fully understand the f...
We want to use this transistor to drive piezoelectric ceramics at 900KHz, 1.7MHz, and 3MHz, which requires about 50W of power.I have the following questions and need help:1. Can this transistor be used at a frequency of 900kHz? Can it only be used in...