Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Driving Peltier with VNH5019A-E

Posted on January 13, 2015 at 20:37I am having trouble driving a peltier device with the VNH5019. The channel config. in the scope pictures is as follows:1. Vin to H-bridge2. PWM logic in3. A leg out4. B leg outGoodDrive.bmp shows what's supposed to...

Using X-NUCLEO-IHM01A1 without an STM32 Nucleo board

Posted on February 11, 2015 at 22:42I'm trying to use an X-NUCLEO-IHM01A1, but without an STM32 board. That is, I need to wire up each of the necessary pins individually, sending the proper signals via another microcontroller.For now, I just need to...

dvelasco by Associate II
  • 689 Views
  • 0 replies
  • 0 kudos

Vbatt Profile - Dump load simulation

Posted on February 04, 2015 at 09:23Hi, would be possible to share a Vbatt file to perform a load dump simulation? (Vbatt nominal:12V). Thank you. Best regards, Marty Beaker #twistersim

brgmrc by Associate
  • 759 Views
  • 1 replies
  • 0 kudos

EVL6699-90WADP Gerber

Posted on January 18, 2015 at 11:44Hello,We are currently evaluating EVL6699-90WADP. Is there anywhere to get the Gerber files for the EVM?Matt

EMC filtering with L6235

Posted on January 07, 2015 at 18:41Hello, Is there a best practice for EMC filtering on the L6235? In applications with other drivers we've added RC filters on the outputs between switches and motor to dampen the switching noise. Is this recommended...

dgrimes by Associate II
  • 1255 Views
  • 2 replies
  • 0 kudos

3PHASELV-KIT max rpm set

Posted on January 03, 2015 at 02:50Hi,Does 3PHASELV-KIT board support a 2 pole motor with 40,000 rpm max speed? the datasheet for 3PHASELV-KIT shows it supports a 6 pole motor up to 3000 rpm, so for a 2 pole motor, I would expect it can support up t...

morteza by Associate II
  • 2745 Views
  • 7 replies
  • 0 kudos

PC based GUIs to operate dspin HW

Posted on January 08, 2015 at 20:54There is no useful information on the ST website (none I can find in three days) that explains which PC GUIs can be used with which eval systems. Can someone explain which PC GUIs are avaliable for which Eval syste...

scope by Associate II
  • 821 Views
  • 1 replies
  • 0 kudos

VN5050 PSpice model

Posted on December 28, 2014 at 17:53Hello all1 I'm searching for VN5050 PSpice model. I saw that the Orcad library for this IC is available. How can I obtain a PSpice model? #vn5050

roman2 by Associate
  • 847 Views
  • 1 replies
  • 0 kudos

L6229 L6235 +5V Supply

Posted on December 03, 2014 at 19:24For EVAL6229 or EVAL6235 with PractiSpin board it looks like 3.3V or 5V reference is from other PCB, is there a way for L6229 or L6235 to supply 5V (for EN, F/R, BRAKE) internally? Does ST make compatible 8-52V to...

dgrimes by Associate II
  • 993 Views
  • 1 replies
  • 0 kudos

EVAL6229PD application notes

Posted on December 02, 2014 at 13:41Hi. I'm trying to find application notes that relate directly to the EVAL6229PD. All I have been able to find is application notes for the EVAL6235N and they do not relate directly to the 6229 as it has a differen...

jc1 by Associate II
  • 1639 Views
  • 3 replies
  • 0 kudos