Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC and interrupt in motor control

Posted on February 07, 2015 at 05:05The original post was too long to process during our migration. Please click on the attachment to read the original post.

problem in compiling code using stsw-stm32100 library

Posted on February 06, 2015 at 19:36hello every body,i generated header files using MC workbench, and then copy them into sys_drive_param folder. then when i open workspace in project folder. it contains only STM32F30x_userpoeject, but according to ...

ijhar09 by Associate
  • 1051 Views
  • 1 replies
  • 0 kudos

Sensorless FOC takeover problem

Posted on October 24, 2014 at 14:44Hi Gigi, I was playing with sensorless rev-up and found a feature not doing what I expected, or maybe also not knowing how to use it correctly. I use Observer+Cordic scheme, and enabled the ''Rev-up to FOC switch-o...

Error in code building

Posted on December 14, 2014 at 11:57hye every body. i m trying to use stm foc firmware 4.0 library. when i tried to build user project example error occured ''Path '.\STM32303C-EVAL\' does not exist !'' can any body help me in order to solve that is...

'overlocking' L6470 / L6472

Posted on April 22, 2014 at 14:31Hi, We have an application with a small steppermotor with only a small load. the current and voltage we use is way too high for the motor for longer periods of time, we only use it in short bursts. The problem is tha...

r2399 by Associate
  • 1181 Views
  • 3 replies
  • 2 kudos

L6470 Daisy Chain (AN3991)

Posted on February 28, 2015 at 13:36Hi There!There's something that I could not understand in the Daisy Chain configuration of the L6470 Stepper Motor Driver. Apart from the SPI Signals and the mechanism of driving each device individually or all si...

Zaher by Senior II
  • 698 Views
  • 0 replies
  • 0 kudos

VIPER17 Startup problem

Posted on February 20, 2015 at 01:33 We are using VIPER17 in our products as a standby power supply for a couple of years in mass production. Recently we faced a problem that if the mains is off and on again this power supply can not start-up. Mains...

lev by Associate
  • 675 Views
  • 0 replies
  • 0 kudos

IC for Traffic Light Led Driver

Posted on February 17, 2015 at 12:55Hi All!!            We are a company based inThessaloniki Greece, which focuses its activities in the sector of trafficcontrol. Our R&D department is in the design process of a power supplydevice that will be used...

sr by Associate
  • 1163 Views
  • 1 replies
  • 0 kudos

About 440VAC to DC converter

Posted on February 15, 2015 at 04:41Hi, I got some information about VIPer06 from google search, it can be applied for 440 VAC input, but the drain current is only 350mA, my requirement is greater than 2A, in ST web site, if I choose VIPer100A-E,   ...

vcchen by Associate
  • 836 Views
  • 0 replies
  • 0 kudos