Finding parameters for L6470
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-04-11 11:13 AM
Posted on April 11, 2014 at 20:13
I am quite novice when it comes to stepper motors and am having some difficulties. I am evaluating the L6470 to replace an old step/dir motor drive. The motor used is an Applied Motion HT17-075 nema17. Form the specs and measurements I have the following data:
phase current 0.85Aphase resistance 6.6 ohmsphase inductance 12mHmeasured Ke 0.0475 V/HzI am driving the motor with a 24V power supply and after going through the BEMF calculations I have a smooth and silent system but top speed is limited to 885 Steps/s . Everything more than that is really noisy and starts to slip.I am set at 128 micro-steps, have the Slew rate at fastest, using voltage compensation and have FS_SPD set to 0x3F. I tried varying the BEMF slopes, and even tried with a 36V power supply but couldn't get it to go faster. I don't have precise numbers but I know that it's really faster with the old drive.What should I try next?thank you! #l6470-speed-param
Labels:
- Labels:
-
Motor Control Hardware
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0