Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STC3115 Questions

Posted on July 26, 2016 at 10:33Hi Sir/Mdm,I have few questions regarding STC3115. After implementation, I have noticed that voltage & current measurements are working properly, however the SOC value is never updated. 1. Is it normal? 2. Does the ST...

VNH2SP30 H-Bridge Unexpected reaction to current control

Posted on March 21, 2016 at 12:33For a project I'm working on I have to be able to switch the polarity of a peltier element (or other device) and be able to linear control the current through the peltier.I didn't want to put a normal relay in this s...

0690X0000060MoZQAU.gif 0690X0000060MoaQAE.gif 0690X0000060MobQAE.gif
jorick by Associate II
  • 943 Views
  • 2 replies
  • 0 kudos

L6924D: How to Derive ICHG from Current Injected in REND?

Posted on August 30, 2016 at 21:00Hello,The datasheet of the L6924D mentions on Page 19 that the the current injected in REND is proportional to ICHG. It also states that the voltage across REND can be used by a microcontroller to check the charge s...

asangare by Associate
  • 627 Views
  • 0 replies
  • 0 kudos

No stabilization of output voltage | SPV1040

Posted on August 30, 2016 at 19:21Hi. I designed the power converter which is supply from the photovoltaic cell ( Umax = 5.5 V / 1 W) on a SPV1040. The problem is that the system did not stabilize the output voltage.The output voltage is proportiona...

0690X00000602gXQAQ.jpg

PowerSTEP01 Manufacturing Delays

Posted on August 18, 2016 at 14:44Hi all.I recently developed a system that uses the PowerSTEP01 devices. I had great trouble getting hold of the devices when I originally prototyped the design. Now I've come to order another batch and no body seems...

howard2 by Associate
  • 595 Views
  • 0 replies
  • 0 kudos

SPV1020 SPI extract data

Posted on August 12, 2016 at 00:39Hi, I design a battery charger with SPV1020 and DN0023. It's works ok. So I connect trought SPI with a uC. I read the different registers succefully. But I want to know what is the scale for register 0x04 (Read Curr...

A6986F current consumption is more

Posted on August 02, 2016 at 08:37Hi All, We are using A6986 ic our board to convert 12V to 5V, but ic itlsef taking more current, its 3.50 mA. Here i am attaching the my part of schematic. Kindly look at it and let me know what may be the problem.

punitb20 by Associate II
  • 817 Views
  • 0 replies
  • 0 kudos

Interfacing STLED316 with Atmega

Posted on August 01, 2016 at 22:00Hello! With Atmega regular hardware SPI, data transfer is 8-bit. Hence, when asserting commands, followed by receiving/transmitting data from/to STLED, each transmission will look like 2 8-bit packets separated by h...

hexel2 by Associate II
  • 1258 Views
  • 1 replies
  • 0 kudos

High voltage input to 7805

Posted on July 29, 2016 at 15:00Hello,We are using L78M05CDT-TR in our design since few years. We are satisfied with the result of product. However we are making new design (PFA) and we considering to use design suggested in datasheet for high volta...

arisence by Associate
  • 1338 Views
  • 1 replies
  • 0 kudos