Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

High voltage input to 7805

Posted on July 29, 2016 at 15:00Hello,We are using L78M05CDT-TR in our design since few years. We are satisfied with the result of product. However we are making new design (PFA) and we considering to use design suggested in datasheet for high volta...

arisence by Associate
  • 1343 Views
  • 1 replies
  • 0 kudos

L6920D breaks after battery insertion

Posted on July 27, 2016 at 11:44Dear all,I'm using an L6920d to generate a 3V3 voltage to power up a circuit from 2 alkaline battery. However it happens that sometimes the component breaks after inserting the batteries (its imput impedance go down t...

matteo2 by Associate
  • 748 Views
  • 0 replies
  • 0 kudos

l6470 Speed Register

Posted on April 15, 2013 at 14:25According to Datasheet Reference:In order to convert the SPEED value in step/s, the following formula can be used:[step/s] = (SPEED X 2 –28)/ tickThat would mean that if I would like to work with step/seconds I hav...

ivlasic by Associate
  • 721 Views
  • 2 replies
  • 0 kudos

Fake STPS20H100CT?

Posted on July 09, 2016 at 13:00Does anybody have an idea, is STPS20H100CT on the photo genuine, or just another one China fake?It is suspicious that it is marked with an unusual for ST font and a circle around ''e3'' is rather an ellipse, but the o...

0690X00000602dOQAQ.jpg
eugene2 by Associate
  • 934 Views
  • 0 replies
  • 0 kudos

L6235 current control

Posted on July 08, 2016 at 15:40Hi i have a problem regarding the L6235PD. With the EVAL6235N everything works fine. Problem is my own PCB layout. The monostable never triggers the bridge off and the motor consumes a lot of current compared to the e...

L6470 When CS goes low pulls SDI down with it?

Posted on July 05, 2016 at 11:11Hi,I have been using an microchip explorer16 board with the EVAL6470H board and working fine. Swapped over to my design PCB and there is a peculiar fault where when the CS pin is high the SDI at the L6470 works normal...

EVAL6470PD Vdd supply and SW input

Posted on June 30, 2016 at 22:42I have two EVAL6470PD boards that I will be using to drive the stepper motors in an XY stage. They will be controlled from a PIC32 board through SPI.  Is there any performance or noise immunity advantage to using an e...

jarratt by Associate
  • 735 Views
  • 0 replies
  • 0 kudos

What kind of impact can demage the L6470pd in that way?

Posted on June 27, 2016 at 13:35Hi at all, is there someone with an idea what has happened there with the L6470. I´ve attached 2 photos of the demaged device and on picture of the scematic sheet. It looks like the motor bridges are directly shorted ...

dbecher by Associate
  • 992 Views
  • 0 replies
  • 0 kudos