PWM: drive output low in disabled mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-04-15 8:57 AM
Posted on April 15, 2014 at 17:57
I'm using TIM1 for a 6-step motor control on a STM32F2xx. According of the table 4 in DM0004234 application note, I update OCxE and OCxNE at each commutation, to select a new step. When OCxE = 0 and OCxNE = 0, the output is disabled. In this case, the output seems to be in high impedance. I would rather have it in OFF-state (low Z). Is there a way to get this result?
Thanks for your help. Simon
Labels:
- Labels:
-
Motor Control Hardware
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-05-05 2:23 AM
Posted on May 05, 2014 at 11:23
Ciao Simon,
For what I know you have to configure the GPIO in output mode and set the proper state (according your polarity) before to set again the same pin for AF. When OCxE = OCxNE = 0 the control of the pin is done back to the GPIO controller. Ciao Gigi