STM706TM MTBF
Posted on January 18, 2018 at 07:02Hi, I'm after the MTBF and FIT data for the STM706TM voltage supervisor.Thanks.#reliability #voltage-regulator
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Posted on January 18, 2018 at 07:02Hi, I'm after the MTBF and FIT data for the STM706TM voltage supervisor.Thanks.#reliability #voltage-regulator
Posted on January 16, 2018 at 13:18Hello,I am using L6472 to control stepper motor. When i apply step clock mode command to L6472 , motor gets hold but during this opertion Motor shaft move by 1 to 2 degree , What is the reason of shaft movement a...
Posted on January 14, 2018 at 20:54I see that there is a difference in the number of microsteps and if they drive/control voltage or current, but is there any other difference? Could please somebody give me a quick comparison between them? I origina...
Posted on January 16, 2018 at 06:35Hello!Can I get the firmware for the STEVAL-ISA172V2?
Posted on December 25, 2017 at 22:38We plan to build a high power PMSM controller based on Stm32f303 (for this motor for a start http://www.thunderstruck-ev.com/motenergy-me1115-brushless-sin-cosine.html).Before we start, we are evaluating the FOC l...
Posted on November 13, 2017 at 14:42Hello,according to the datasheet of the LED1642 driver, the LE signal value is defined by the number of CLK rising edges when the LE is 1.In the datasheet, the figures always show LE signals which are aligned to t...
Posted on January 12, 2018 at 10:32Hi All; I would like to use STPM33/34. How can I use it?. And Where is an example?#current-measurement #stpm33 #stpm34 #stpm3x
Posted on December 02, 2017 at 02:25Hi,I've got some problems in getting the max Current capability of 30A out of the Chip. As soon as the Current goes above 20A the Chip will sooner or later switch of Halfbridge B. I think the problem is to get the...
Posted on December 14, 2017 at 11:33Hi!How many BLDC motors can I control using the STSPIN32F0/ STSPIN32F0A simultaneously?
Posted on January 09, 2018 at 09:38Hello community,i got a problem when i want to create on my stm8 eval board a pwm signal with 350khz and variable duty cycle from 0-100.i calculate the the values for the registers as follows:PWM Frequency = Clock ...