cancel
Showing results for 
Search instead for 
Did you mean: 

Using multiple L6472 ICs on same circuit board

Martiska.Greg
Associate III
Posted on March 25, 2016 at 14:04

I am working on an application where I need to use three L6472 ICs on the same board. I am wondering what external components can be shared between 2 or 3 L6472's. For example, can one cap elec 100uf 63V on the VS inputs (as on your evaluation board) be shared between IC's? What about the charge pump caps and diodes for the VBoot? I am looking to reduce components and layout space as the total board size is restricted for this application. For information, the motor voltage will be 12V and the typical motor current will be less than 1 amp. Also only one motor will be running at any one time.

Thanks for your help.

Greg

#l6472
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0