3-phase BLDC motor interface using STSPIN32F0A
Posted on December 14, 2017 at 11:33Hi!How many BLDC motors can I control using the STSPIN32F0/ STSPIN32F0A simultaneously?
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Posted on December 14, 2017 at 11:33Hi!How many BLDC motors can I control using the STSPIN32F0/ STSPIN32F0A simultaneously?
Posted on January 09, 2018 at 09:38Hello community,i got a problem when i want to create on my stm8 eval board a pwm signal with 350khz and variable duty cycle from 0-100.i calculate the the values for the registers as follows:PWM Frequency = Clock ...
Posted on January 06, 2018 at 01:24Three questions regarding MC_SixStep_Ramp_Motor_calc()1.) What unit do the mechanical acceleration rate parameters/variables have? (apparently not 1/min/s or rad/s²)2.) 'mech_accel_hz = SIXSTEP_parameters.ACCEL * ...
Posted on January 04, 2018 at 18:11Hi,I have just started working on a configuration wizard utility in Keil uVision for the setup of stepper motors.As can be seen, the configuration wizard so far setups the acceleration, deceleration, maximum and mi...
Posted on December 28, 2017 at 12:28Hi!Fatal error: Slected core ( Cortex-M3) is not same as the target core ( Cortex-M0)Session aborted!With STEVAL-SPIN3202, even the compile goes well, and the above error occurs on the link. I do not know why. Tha...
Posted on December 18, 2017 at 03:40 I brought a 'STEVAL-SPIN3202'. It based 'STSPIN32F0A'.But main-chip written as follows.-----------------------------------------SPIN32F0FN02U A5THA 11 722ST @ A-----------------------------------------Is this 'ST...
Posted on June 24, 2017 at 22:25I'm using the SPIN3201 eval board and have had it working in sensor-less and Hall modes, but i'm looking for better low very low speed, < 10 rpm behaviour where the halls don't produce smooth torque. I've attached a 1...
Posted on October 31, 2017 at 01:26There seems to be an error in either the datasheet or the applicatio note of the STC3117 gas gauge.The error is in the bit description of the REG_MODE register, specifically the VMODE bit. The datasheet says the fo...
Posted on December 13, 2017 at 10:28At the maximum, how many BLDC motors can be controlled using one STSPIN32F0A?If I happen to use only Brushed DC Motors, how many such DC motors can be controlled simultaneously using one STSPIN32F0A? #motors #moto...
Posted on December 13, 2017 at 08:36Hi. I would like to set a battery float voltage to 4.1v (to extend the life of the battery). Looking at the datasheet for the li-ion battery charger STBC02, it looks like this can be adjusted but 4.2v seems to be ...