cancel
Showing results for 
Search instead for 
Did you mean: 

L9942 Set Up

davida.boling9
Associate
Posted on March 18, 2016 at 20:15

In the datasheet, Register 0 has 5 bits (P0-P4) that are defined as ''This bits control position of motor, e.g. 00000 step angle is 0, 01111 step angle is 180.  There is no table which defines how to derive the other angles.  Are these bits incremented each time STEP is switched?  What are the purpose of these bits?  I will be full-stepping the motor in all circumstances.  It is a 20 step/revolution motor.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0