Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

losing bits when reading ABS_POS from L6470

Posted on March 09, 2015 at 08:41Hi, I am facing an issue where it seems the L6470 drops the most-significant bit of each byte transferred when I GetParam ABS_POS. Here is a screenshot of the SPI comminucation during the last byte transferred when t...

0690X00000603PNQAY.jpg
jasonlee9 by Associate II
  • 1846 Views
  • 3 replies
  • 0 kudos

STWLC03 wireless receiver tuning mistakes

Posted on February 07, 2018 at 17:52Hi,I want to compute the resonant circuit formula to have the right value for C :I use the STEVAL-ISB039V1 kit with transmitter and receiver boardFirst mistakes with inductive and capacitors values :If I use the f...

POWERSTEP01 in StepClock Mode

Posted on January 01, 2018 at 12:06Stepper Motor Driver IC POWERSTEP01:We implemented  POWERSTEP01 on our own PCB.We are sending command to POWERSTEP01 through on board STM32F072 microcontroller through SPI.When we send StepClock  command with direc...

Performance with voltage mode on powerSTEP01

Posted on June 23, 2017 at 05:53I'm testing the powerSTEP01 with http://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-move-actuate-hw/x-nucleo-ihm03a1.html connected Ardui...

0690X00000602TiQAI.bmp

Stall Detection in L6472

Posted on January 27, 2018 at 10:11Is it theoretically possible to use the stall detection in the L6472? According to the data sheet, this function is not available, but what if I write the register h14 and read the status register (bit 13, bit 14)?...

STM706TM MTBF

Posted on January 23, 2018 at 22:55Hi, I'm after the MTBF and FIT data for the STM706TM voltage supervisor.I've already asked this but the person responding somehow messed up the answer by tying it an email address that doesn't have an account so th...

STC3115 Adjusting Configuration

Posted on January 30, 2018 at 00:22After reading the STC3115 datasheet (D023755 Rev 8) and system integration (AN4324), plus FAQ and the driver code on GitHub, I have questions about the REG_VM_CFG, REG_CC_CFG, REG_VM_ADJ and REG_CC_ADJ.Are the *_CF...