Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi all, We are new here. We are thinking of using ST L6203 motor drivers on our robots and are wondering if it is recommend to control motor speed by PWN on the enable pin or is better to PWN either IN1 or IN2 depending on direction.

http://users.ece.utexas.edu/~valvano/Datasheets/L6203.pdf We've had quiet a discussion about this and it would be great to know which method is preferred.CheersTerry

TSmit by Associate
  • 975 Views
  • 1 replies
  • 0 kudos

Opto-coupler for L6470 ?

Posted on May 21, 2018 at 16:33It is necessary to apply a opto-coupler between an SPI Master and the L6470 circuit on the X-NUCLEO-IHM02A1 board ? I could not find any information about galvanic isolation in L6470 documentation.#x-nucleo-ihm02a1 #op...

Driver selection for High Power LEDs

I'm currently working in a project where I need to control the intensity of 24 high power LEDs in 5 levels. I'm planning to use LumiLeds L1CU-BLU1000000000 (https://www.lumileds.com/uploads/705/PB198-pdf) where the cut-off voltage is 2.83 volts and c...

RMeno by Associate
  • 863 Views
  • 0 replies
  • 0 kudos

L6482, BEMF spikes

Hi,I'm using L6482 Stepper motor driver and I'm capturing BEMF spikes that can be up to +/-17V above VS and GND.It been measure at the OUT1A to GND.Is it acceptable? It is not clear in datasheet.Also I don't see any protection devices requirement su...

How to recharge a lead battery in UPS mode

Hello, I would like to recharge a lead battery (6V - 4500mAh) by using two different sources : a solar pannel and/or a micro USB input. The device needs to run in UPS mode (uninterruptible power supply). Do you know if ST proposes some IC that could ...