Posted on April 24, 2017 at 13:15I am using L9823 in my design to drive the outputs. I also want it to behave as input so that I can connect IO module. How can I use it as input?Thanks in advance
Posted on April 24, 2017 at 13:14I am using L9823 in my design to drive the outputs. I also want it to behave as input so that I can connect IO module. How can I use it as input?
Posted on May 16, 2017 at 05:22As L9823 is an output driver IC, I wanted to use it as input also. I need to connect IO devices in my design on same line. i.e. the user can change the module as per his requirement from Input to output or vice versa. ...