Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

No reply

I think the STM group not at all replying the people questions. May be they are not having interest to their followers.

GKris by Associate
  • 793 Views
  • 0 replies
  • 1 kudos

Using a Viper12 to run leds over 50-1000V range

Hi im struggling with a circuit im designing, im trying to run 3x 24V indicators using a Viper12 circuit. Ive set the circuit up as below:The idea is that the pre circuit introduces the Zeners at 650V, offsetting the input to the Viper circuit by 400...

0690X0000060RyUQAU.png
bsav by Associate
  • 867 Views
  • 1 replies
  • 0 kudos

Automotive rated part or not ?

Hi all,Can anyone please confirm if the following parts are AEC-Q qualified or not?VNH7070ASTRVNH5050ATR-EVNS3NV04DP-EVND5E006ASPTR-EVNQ7050AJTRThanks in advance.Regards,Saikumar

SNata by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

Some questions about MCSDK 5.1.1. (etc. Motor)

Posted on June 25, 2018 at 03:34Now I try to control the BLDC motor with ICS.There is no example for ICS. : DAsk the STM Forum members.SpecificationsMCU: STM32F427VGIPM: STGIB15CH60TS-LCurrent Sensing IC: AMC1200 (FDA) (Isolation)Motor current phase...