Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Seeking Info on STEVAL-WBC2TX50

Hello STMicroelectronics Community,I'm working on a project using the STEVAL-WBC2TX50 evaluation board and would greatly appreciate any information or insights you can share. I currently have the PDF schematics from https://components101.com/sites/de...

Resolved! VNHD7012AY Evaluation Board

Hello everyone, I'm looking for a Motor Driver IC and Motor Driver Evolution Board that can deliver 15 amps of continuous current. The VNHD7012AY Evaluation Board seems suitable for me, but will STM provide support in the future? Or are there any oth...

ufukv by Associate II
  • 798 Views
  • 3 replies
  • 4 kudos

Resolved! {19368485} Top marking for LDO L78L33ABUTR

Dear Respected Sir/Madam,Could you kindly confirm if the top marking 9C220 on the received LDO with Part Number: L78L33ABUTR is correct?As per the catalog information, the expected top marking for this LDO appears to be 8A.For your reference, I have ...

Resolved! ViperPlus Series for DCDC

I am trying to build a DCDC Converter with following conditionsVin: 400~600VDCVout: 12~15VDC(Isolation is not required)Current Rating: 100mA~300mA(Not really stricted)I can see DC application simple schematic at the first page of the datasheet for Vi...

Resolved! Convert PB battery charger for LiFEPO4 batteries

Hi!I have an electric scooter that's a few years old, and I'm trying to find out if it's possible to use its charger for LiFePO4 batteries. The scooter's original batteries are two lead-acid units connected in series (24V total)The charger has the re...

Rafao95 by Associate
  • 718 Views
  • 1 replies
  • 0 kudos

Resolved! STC3100 Current register nonsense values

Hi, I am having the same issue as this previous forum post, but the question was never answered.  Voltage and temperature sense give expected readings. REG_VOLTAGE_LOW: 29; REG_VOLTAGE_HIGH:6 --- VOLTAGE: 3818mVREG_TEMPERATURE_LOW: 186; REG_TEMPERATU...

rs231 by Associate II
  • 966 Views
  • 5 replies
  • 0 kudos

Resolved! STWLC38 FCC test settings

Hello expert,We are developing a product using STWLC38 and are currently trying to obtain FCC certification.In order to perform the test, the following is required by the testing agency.・To output a continuously ASK modulated signal. (We only use BPP...

Ryoma by Associate III
  • 1446 Views
  • 4 replies
  • 1 kudos

SPICE model for LDFPVR ?

Your products have been instrumental in helping us achieve remarkable advancements, and we truly appreciate the quality and support you provide. I am currently developing VHF PA  circuit that incorporates your product, the LDFPVR . To validate the de...

SRK2000A: IC skips the gate pulses.

Hi,  We are working on LLC converter Vout=12V; Pout=100W. We are using SRK2000A IC at the output. We are facing some issues related to it. The IC behaves as expected while driving the load from 30% to 100%. But when we start reducing the load below 3...

download.png download.png
PKulk by Associate
  • 828 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.